Grundfos offers huge savings for amusement parks

03/03/2016

Grundfos offers huge savings for amusement parks

Showcasing its energy efficient pumps at IAAPI Amusement Expo 2016

 

Mumbai, March 3, 2016: Grundfos Pumps India Pvt. Ltd. (Grundfos India), one of the leading pump manufacturers in India, is participating in the 16th edition of IAAPI Amusement Expo 2016 in Mumbai. The three day expo scheduled from March 3rd to 5th aims at providing a platform to discuss innovative ideas, trends, schemes and learning experiences related to the amusement industry. 

Pumps are widely used at amusements parks for water supply, raw water intake, fountains, water rides, surf rides, water treatment and sewage effluent handling. These pumps are unseen energy users wither due to inefficiencies or over-sizing. To help amusement parks Grundfos offers high energy efficient pumps that reduce energy consumption, lower carbon emissions resulting in cost savings. 

Grundfos India has a wide range of innovative and efficient pumps for water processing, water treatment and safe pumping solutions. The company is exhibiting its single-stage centrifugal pumps that efficiently circulate the processed water while its range of unmatched end suction pumps ensure safe pumping at amusement parks. 

The Grundfos SP range of submersible pumps are renowned for their high efficiency and reliability. SP pumps represent state-of-the-art hydraulic designs that is built to deliver optimum efficiency during periods of high demand. These pumps provide low long-term costs and high operating reliability regardless of the application. 

Grundfos is also showcasing its CR Range and NB / NK range at the expo. The CR range of pumps can be applied in almost any industrial and domestic solutions such as process water systems, washing and cleaning systems, swimming baths, etc. The stainless steel NB / NK end-suction pumps are specifically made for demanding environments like amusement parks. Technical feature like dedicated single, tandem or back-to-back shaft seal arrangements are available to accommodate the specific nature of whatever is running through the pipes and to ensure leak-free and safe pumping of even hazardous or explosive liquids.

Commenting on the occasion, Gangaprasad G, Vice President- Sales
(Building Services) Grundfos India, said, “Amusement parks are constantly evolving to become more innovative and competitive. One of the ways of staying ahead in this industry is to ensure minimized operating expenses. It is also increasingly becoming important for amusement parks to be more sustainable and reduce their environmental impact. We at Grundfos realize this and are working with amusements in the country and the world over to help them move to intelligent and energy efficient pumps. By doing so we are helping them not only save costs but the planet as well.”

Visit Grundfos India at the expo: Stall no. F9, Bombay Exhibition Centre, Mumbai.

About Grundfos India:

Grundfos Pumps India Pvt.  Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established in March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 20 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply,
domestic water supply, sewage and wastewater, dosing, chlorination systems,
disinfection systems and pumps running on renewable energy.

For more information, visit: http://www.grundfos.in/

 

  

 





    Facebook Twitter LinkedIn Technorati