Seminars to Showcase the Leading Pumping Solutions for Commercial Buildings

29/04/2014

Seminars to Showcase the Leading Pumping Solutions

Seminars to Showcase the Leading Pumping Solutions for Commercial Buildings

Chennai, India, April 29, 2014: Grundfos Pumps India Pvt. Ltd (Grundfos India) will be hosting seminars to showcase its leading pumping solutions for the commercial buildings segment across multiple cities. To ensure optimal comfort and safety without compromising energy consumption, Grundfos has a wide range of pumping products to suit the various commercial building application needs.

These seminars will be most relevant for builders, developers, consulting engineers, architects, project managers, facility managers, hoteliers, contractors and service providers in building services industry. Some of the key Grundfos products that will be displayed and demonstrated during the seminar include:

MAGNA 3 - It is the most energy efficient circulator pump in the air-conditioning market. The new Magna 3 circulator pump gives the user and integrated solution combining a pump, balancing valve and a BTU meter. Magna3 is a perfect fit for radiant heating and cooling application where it eliminates most of the field instrumentation.

Hydro MPC - Grundfos Hydro Booster System provides dependability, supreme technology and ease of operation for a range of purposes. The Grundfos Hydro Booster system is equipped with Multi Pump Controller (MPC) which ensures systems are operated as optimally as possible. Grundfos Hydro Boosters with MPC systems offers unique frictional loss compensation algorithms which save up to 10% over constant pressure based Hydro booster systems.

SE/SL - Grundfos SE/SL are highly dependable, powerful sewage pumps designed for handling unscreened raw sewage. These SE/SL pumps with the ground breaking S-tube impeller offers efficiencies up to 80% through its tube shaped channel impeller design. These pumps are acknowledged for their strength, durability, and for innovative features such as smarter impeller clearance adjustment system and smart seal for leakage prevention.

SQ & CR Flex - Grundfos Solar submersible / surface pumps provide perfect sustainable, reliable and cost efficient alternative to regular water transfer solution in a commercial building. With it’s in built flexibility, to operate in both AC and DC voltage supply, these pumps offer unique solution to end customers.

These seminars will be held in Trivandrum, Raipur, Bhubaneswar and Lucknow

Date & Day Venue / City Contact Person
Friday, May 9, 2014 Trivandrum Santhosh KG: +91 9895758124
Friday, May 30, 2014 Raipur Debatosh Mishra: +91 9937034044
Friday, June 13, 2014 Bhubaneswar Debatosh Mishra: + 91 9937034044
Friday, June 27, 2014 Lucknow Minhal Abbas Rizvi: +91 8953111110

The programme will start at 7:30 pm on each day and will be followed by dinner. For more information on these seminars and to register, you can contact the above listed Grundfos India focal points:

About Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established in March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 20 offices across India. Grundfos India provides pumps and pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy. For more information, visit http://www.grundfos.in/

For editorial queries, please contact:
Mahathi Parashuram
Head – Public Affairs
Grundfos Pumps India Pvt. Ltd
Email: mahathi@grundfos.com
 Mobile: +91 9600063482





    Facebook Twitter LinkedIn Technorati