Grundfos India supports dewatering efforts in Chennai

11/12/2015

Grundfos India supports dewatering efforts in Chennai

Grundfos India supports dewatering efforts in Chennai

Chennai, December 11, 2015: Grundfos India has been working closely with the Chennai City Corporations and corporations to dewater the flooded areas in the city. The water inundated at Olympia Tech Park, Villivakkam, Ambattur, Mogappair, Semmancheri, Sholinganallur,  were pumped out  by providing Grundfos’ mobile pumping station (MPS 101) specifically designed for floods. The pumps are now stationed at DLF Tech Park to remove water from their campus. The pump helped in reducing the water that was logged up to waist deep in few of these areas and up to 8 ft feet at Olympia Tech Park. Grundfos India’s mobile pumping stations worked effectively in dewatering these flooded areas.

These mobile pumping units are dewatering pumps which can discharge around two lakh LPH. Grundfos India has two of these pumps that discharge a total amount of 4 lakh LPH. The advantage of using this pump is that it can run on both diesel and electric power as it has a capacity of 63kVa Genset. Also this entire unit can be towed to any place and the pumps can be positioned at any level with the help of an inbuilt crane.

Commenting on these efforts of Grundfos India, Balaji Seshadri, Head – Service & Engineering (Mechanical & Tech support) said “These pumps and systems can play a critical role in ensuring that areas or even corporate campuses do not flood. The process is simple and mobile that can be used to dewater flooded areas easily and quickly”.

About Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established in March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 20 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy. For more information, visit: http://www.grundfos.in/

For editorial queries, please contact:

Mahathi Parashuram

Head – Public Affairs & Marketing

Grundfos Pumps India Pvt. Ltd

Email: mahathi@grundfos.com





    Facebook Twitter LinkedIn Technorati