Grundfos SCALA2: Perfect water pressure in an all-in-one unit

21/12/2016

Grundfos SCALA2: Perfect water pressure in an all-in-one unit

Chennai, December 21, 2016: Grundfos India, today launched SCALA2, which is a fully integrated water booster pump. The SCALA2 provides perfect water pressure in all taps at all times – even with multiple taps and showers running at the same time. It packs pump, motor, tank, sensor, drive and non-return valve into one compact unit. With its intelligent pump control, SCALA2 automatically adjusts performance to both inlet pressure and water consumption in the home. Thanks to a water-cooled motor, SCALA2 even offers one of the lowest noise levels of any booster on the market.

 

What is intelligent pump control?

SCALA2 features a built-in sensor, which constantly measures the discharge pressure. If the pressure drops below the desired level, SCALA2 boosts its operation immediately to compensate for the loss of pressure. We call it intelligent pump control and the result is perfect water pressure.

 

Benefits

§  Perfect water pressure: Intelligent pump control adjusts operation automatically

§  Low noise: As quiet as a modern dishwasher (47 dB(A) in typical use)

§  Easy selection: One variant for all domestic boosting needs

§  Easy installation: Compact, all-in-one solution, plug-and-pump

§  Easy to operate: User-friendly control panel

§  Reliable operation: Dry-running protection, anti-cycling

§  Long lifetime: Quality-tested to perfection, maintenance-free

 

Applications

SCALA2 is the perfect choice for residential buildings with up to 3 floors and 8 taps.

§  Boosting from tanks: Increases water pressure from roof tanks, break tanks and ground tanks, including rainwater tanks.

§  Boosting from wells: Pumps water from a depth of 8 metres

§  Suitable for both Indoor and outdoor installation

 

Commenting on the launch of SCALA2, Ranganath N. K., Managing Director, Grundfos India said, “We at Grundfos India are proud to launch the perfect water pressure pump, SCALA2.  The SCALA2 is a fully integrated water boosting solution designed for easy installation and operation. It is compact enough to fit inside a kitchen cupboard, is very quiet and it covers all domestic boosting needs. SCALA2 is an extremely reliable and robust booster pump for homeowners”.

 

About Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established on March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 14 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy. For more information, visit: http://www.grundfos.in/

 





    Facebook Twitter LinkedIn Technorati