Efficient Water Management: A Key to Building Smart Cities

04/09/2017

Efficient Water Management: A Key to Building Smart Cities

Efficient Water Management: A Key to Building Smart Cities

New Delhi, September 4, 2017: The Smart Cities campaign has been high on India’s agenda as this is perceived as the step towards building a sustainable and developed country. A smart city needs to have an environment that is suitable to accommodate the requirements of the progressive urban population such as transportation, connectivity, uninterrupted power and water & wastewater management to name a few. 

According to Indian Ministry of Urban Development, 60% of India’s population will live in cities by 2050. This means that there will be stress on our cities to deliver
more services with limited resources. With India’s rapid urbanization and growing population, water demand has already exceeded the supply. A smart city will need to ensure 24*7 uninterrupted supply of water for its development, which may not be possible if the current scenario persists. Therefore, it is very important to take measures to secure water through efficient water management systems. 

Grundfos India, one of the leading pump manufacturers in India, is therefore promoting the importance of efficient water management systems in building smart cities at the ‘3rd Water Innovation Summit 2017’ organized by Confederation of Indian Industry (CII). “Smart Water Management: A Key Building Block of the Smart Cities & Villages of the Future” is the theme of this two-day summit taking place on September 4 and 5, 2017 in New Delhi. Grundfos India is the gold sponsor of this Summit.

Intelligent water management systems are critical to making Smart Cities successful. According to a WRG report, there are situations in which 40% or more of the water that is pumped into a distribution grid is lost before it ever reaches the consumer in cities across the world. The report goes on to state that many cities have also found that if they simply reduce water pressure in the grid, they also reduce leakage and minimize wear and tear on aging pipes. Such issues can be addressed by ‘smart’ technologies such as Grundfos’ Demand Driven Distribution pressure control system, which  can save both water and money by delivering optimal water pressure at any given time. This system can automatically monitor grid use patterns with remote sensors and adjust the water pressure accordingly using a Grundfos software algorithm. It reduces both water and electricity consumption by up to 20%, and water pipes will last longer because they are less likely to crack. The return on investment is short and in some cases down to a year.

Commenting on smart water management solutions for Smart Cities, Gaurav Mathur, Head - Business Development (Building Services) at Grundfos Pumps India Pvt. Ltd said, “Smart water management is definitely the key building block of the Smart Cities of the future. Therefore, it is critical to invest in the right solutions and technologies. We need water management systems that are sustainable, reliable, energy efficient and above all intelligent”. 

About Grundfos India: Grundfos Pumps India Pvt. Ltd.(Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established on March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan, Maldives and Nepal. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 14 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy.

For more information, visit: http://www.grundfos.in/


    Facebook Twitter LinkedIn