Grundfos India exhibits its advanced energy- efficient pumps at ACREX 2016

25/02/2016

Grundfos India exhibits its advanced energy- efficient pumps at ACREX 2016

 

Mumbai, February 25, 2016 – Grundfos Pumps India Pvt. Ltd. (Grundfos India), one of the leading pump manufacturers in India, is participating in the 17th edition of ACREX 2016 in Mumbai. The three day expo scheduled from February 25 to 27 will focus on the ‘Infinite Opportunities for HVAC&R and the Building Services Industry’.

As per the Indian Society of Heating, Refrigerating and Air Conditioning Engineers (ISHRAE), the HVAC industry is expected to reach Rs.20,000 crore by 2016, and the sector is expected to witness nearly 15-20 per cent growth y-o-y. The growth is
anticipated due to increase in construction activity in infrastructure and real
estate sectors. The industry is set to witness immense competition as customers
are price sensitive and looking for affordable energy-efficient systems due to
the rising energy costs and environmental awareness

Grundfos India has a wide range of intelligent and efficient pumps and solutions for air conditioning, refrigeration and building services. The company is exhibiting its intelligent in-line pump TPE3, designed specifically for use in heating and cooling systems for commercial buildings. With its built-in heat energy meter and flow limiting function, the pump totally eliminates the need for a pump throttling valve. This pump is exceptionally energy efficient In-line pump choice, exceeding industry standards.

Along with TPE3, Grundfos is also showcasing MAGNA3, the most proficient circulator available in the market today. The MAGNA3 is designed to offer a complete range of control mode options expected from a state-of-the-art circulator pump. AUTOADAPT and FLOWADAPT, the two intelligent modes set MAGNA3 apart from the competition.

Commenting on the occasion, Gangaprasad G, Vice President- Sales
(Building Services) Grundfos India, said, “We are witnessing an increasing demand for an effective pumping solution to reduce energy costs and environmental impact. Our pumps are designed and developed to highlight Grundfos’s commitment to our customers’ and the industry’s need for intelligent automatic solutions that minimizes the lifecycle cost of the pump, reduces operational cost and enhances sustainability efforts.”

Visit Grundfos India at the expo at Stall no.H1C – 9A, Bombay Convention and Exhibition Centre (BCEC), Mumbai.  

 

About Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established in March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 20 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy.

For more information, visit: http://www.grundfos.in/

 

For editorial queries, please contact:

Mahathi Parashuram                                 

Head - Public Affairs & Marketing                   

Grundfos Pumps India Pvt. Ltd.          

E-mail: mahathi@grundfos.com





    Facebook Twitter LinkedIn Technorati