Grundfos India launches Chlorine Dioxide Production System

15/05/2015

Grundfos India launches Chlorine Dioxide Production System

Grundfos India launches Chlorine Dioxide Production System

Hyderabad, May 15, 2015 – Grundfos Pumps India Pvt. Ltd. (Grundfos India), one of the leading pump manufacturers in India, and a subsidiary of the Danish pump giant Grundfos Holdings, launched its Chlorine Dioxide Disinfection System for water treatment applications. This efficient system can be used for treating cooling tower water, industrial raw water, process water and drinking water.

Based on underwater generation technology, the system generates chlorine dioxide (ClO2) using concentrated solutions of sodium chlorite and hydrochloric acid. With their high precision, integrated Grundfos dosing pumps the system assures a high performance level and yield. This innovative product from Grundfos is a customized system for the generation of 1 kg to 200 kg ClO2/hour.

The Grundfos chlorine dioxide system can be tailor-made according to customer needs: titanium pumps for pressurized injection, a distribution panel for multiple injections, complete or partial redundancy, external communication for remote control, etc. It is designed with very effective underwater generation technology which not only consumes lesser chemicals, but also generates lesser by-products.

The small volume of reaction chamber of the Grundfos chlorine dioxide system means lower ClO2 quantity, and therefore lower risk. There is no risk of concentrated ClO2 gas getting released into the atmosphere as the highly concentrated ClO2 is generated underwater. If it is not possible to install the system indoors, or if ambient conditions are not suitable for an outdoor installation, the dosing section and the control system can be preinstalled in an air-conditioned container.

Commenting on the occasion, Shankar Rajaram, Head - Industry (North & South), Grundfos India, says, “We have launched this product with an objective to have the least impact on the environment and at the same time ensure maximum safety. We are confident that this product will be valued by the user industry and benefit the customers alike.”

About Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established in March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 20 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy. 

For editorial queries, please contact:

Mahathi Parashuram
Head - Public Affairs
Grundfos Pumps India Pvt. Ltd.
E-mail: mahathi@grundfos.com

 

 





    Facebook Twitter LinkedIn Technorati