Grundfos India Launches High-Efficiency Hydro MPC Pumps with IE5 Motor

26/09/2017

Grundfos India Launches High-Efficiency Hydro MPC Pumps with IE5 Motor

Grundfos India Launches High-Efficiency Hydro MPC Pumps with IE5 Motor

Chennai, September 22, 2017: Grundfos India, one of the leading manufacturers of energy-efficient pumps, today announced the launch of its new range of Hydro MPC pumps with the IE5 Motor. The Grundfos Hydro MPC booster systems are of very high standards and combiningthis with the IE5 motor, which is integrated with a frequency converter, connects the accumulated pump experience of Grundfos into the dedicated control software. This combination of pump and customizable software optimizes your system’s performance for any load point, delivering an unsurpassed reduction of energy consumption. As an industry pioneer, Grundfos is excited to introduce the IE5 Motor, which helps in energy conservation of up to 7 per cent and a reduction in the payback time of these controlled pumps.

The Grundfos Hydro MPC booster systems are designed to last and are sturdy. The compact units also enables easy access to all service parts. Grundfos Hydro MPC booster systems can be used wherever additional pressure is required. Some of the key features and benefits are:

  • Reliable highly efficient
  • Highly efficientService-friendly
  • Space-saving
  • Easy to commission
  • Perfectly adapting to the flow
  • Low-flow detection
  • Application-optimized software

Assuring an unprecedented level of performance, the Hydro MPC motor is unparalleled with its state-of-the-art intelligent components. The Hydro MPC pumps with IE5 Motors will be available with systems that are pre-configured from the factory with variety of pump sizes to increase water boosting. 

Commenting on this launch, G Ganga Prasad, Vice President – Sales (South), Grundfos India, said, “In every high performing building there is a high performing pump. But pumps are only part of the story. Intelligent & integrated solutions allow you to take control of your entire system to achieve an even higher performing building. With intelligent pumps, design and high efficiency IE5 motors, Grundfos is raising the bar to ensure exactly this”.

About Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established on March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan, Maldives and Nepal. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 14 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy. For more information, visit: http://www.grundfos.in/

 


    Facebook Twitter LinkedIn