Grundfos India reinforces the need for intelligent plumbing practices for commercial buildings

21/03/2016

Grundfos India reinforces the need for intelligent plumbing practices for commercial buildings

~Company is the gold industry partner at the Indian Plumbing Conference 2016~

Jaipur, March 18, 2016 – Grundfos Pumps India Pvt. Ltd. (Grundfos India), one of the leading pump manufacturers in India, is participating in the 21st edition of Indian Plumbing Conference 2016 in Jaipur. The two day conference scheduled for March 18th and 19th will focus on ‘Water conservation through good plumbing practices’.

 

Plumbing is a crucial part of any building. With the increasing need for sustainable solutions and the only way forward is smart plumbing practices to make buildings smart. Currently, plumbing practices are underrated and there is a need for paradigm shift to offer the best integrated-comprehensive solutions.  The driving factors are energy efficiency, right choices of ancillary products and maintain international standards to ensure leakages, pressure fluctuations and wastage can be curbed to conserve water and energy.

 

Grundfos India has a wide range of intelligent and efficient pump solutions that help reduce the excess water and energy usage for every application in buildings. Grundfos  has a holistic system approach with components that adapt to requirements in areas like wastewater, water boosting, heating system, chilled water system and fire safety.

 

The company is exhibiting its SE and SL pumps, high wastewater pumping solution that come with smart trim technology and are designed for handling wastewater, process water and sewage in heavy-duty municipal, commercial, industrial and domestic applications. These wastewater pumps offer the best total, wire-to-water efficiency and are available with efficient S tube channel. With the     S tube impeller, the pump efficiencies can go up to 83.4%.

 

Grundfos guarantees variable pressure with its reliable water pressure boosting system, Hydro MPC boosters which will be showcased at the conference. The sturdy, efficient and compact Hydro MPC booster pumps are made to handle even the most difficult boosting jobs with ease and accuracy. It’s the most energy-efficient and reliable booster system pump choice, exceeding industry standards. Having been designed to meet specific customer demands for capacity and control, Hydro MPC can be used wherever additional pressure is required.

 

Commenting on the occasion, Gangaprasad G, Vice President - Sales (Buildings) said, “There is a growing need for water and energy conservation to meet the predicted scarcity of these key resources. An essential aspect to improve efficiency and minimize costs is to adopt intelligent pump solutions. Grundfos pumps are the industry's most efficient pumps for commercial building applications.”

 Visit Grundfos India at the conference at Stall no. 3, Hotel Clarks Amer, Jaipur.

 

About  Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established in March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 20 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy. For more information, visit: http://www.grundfos.in/

 

For editorial queries, please contact:

Mahathi Parashuram                                 

Head - Public Affairs & Marketing                            

Grundfos Pumps India Pvt. Ltd.                

E-mail: mahathi@grundfos.com