Grundfos launches BMS hs AC, a lightweight ultrafiltration booster module in India

07/06/2016

 Grundfos launches BMS hs AC, a lightweight ultrafiltration booster module in India

Grundfos launches BMS hs AC, a lightweight ultrafiltration booster module in India

New features aim to considerably reduce maintenance hassle and pump downtime

Chennai, June 6, 2016: Grundfos Pumps India Pvt. Ltd. (Grundfos India), one of the leading pump manufacturers in India, today announced the launch of its energy efficient BMS hs AC high speed booster pump for reverse osmosis and ultrafiltration applications in India. The pump ensures high efficiency and energy savings due to it improved design and enhanced features.

 The BMS range is a completely new range of booster modules mainly used for reverse osmosis and (ultra) filtration applications that improve efficiency compared to earlier ranges. This range of lightweight, ultra-filtration booster modules are directly coupled pump powered by an external motor. With the increasing demand for sustainable and energy efficient pumps in the water treatment segment, these ranges of pumps are specifically designed to improve efficiency and for high flow and pressure applications. 

The new BMS hs AC, is a high-speed booster pump with an asynchronous motor, that can generate an outlet pressure of up to 82.7 bar and is designed for applications where high outlet pressure is needed. These pumps can be integrated in any water treatment system and have a very small footprint. The pumps’ vital components that touch water are made of super duplex stainless steel and can withstand a maximum temperature of 60 degrees Celsius.  

The BMS hs AC pumps are designed for various applications like:

  • Water Treatment plants
  • Ultra-filtration in chemical and galvanic industries
  • Hospitals and laboratories
  • Industries like chemical, electronics, minerals and metal
  • Painting workshops
  • Reverse Osmosis water supply systems
  • Pressure boosting
  • Liquid transfer

Commenting on the launch Saravanan Panneer Selvam, Chief Operating Officer – Sales, Grundfos India, said, “The launch of BMS hs AC is a reflection of Grundfos’ constant dedication to increase our products’ efficiency and sustainability. We are certain that the demand for energy efficient and reliable pumps will help ensure the success of this product like any other product Grundfos has launched in India”.

About Grundfos India:

Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly owned subsidiary of Grundfos Holdings was established in March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan and Maldives. Currently, Grundfos India has more than 250 employees and works with 200 distributors and dealers with 14 offices across India. Grundfos India provides energy efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply,
domestic water supply, sewage and wastewater, dosing, chlorination systems,
disinfection systems and pumps running on renewable energy. For more information, visit: http://www.grundfos.in/

For editorial queries,please contact:

Mahathi Parashuram                                 

Head - Public Affairs & Marketing                 

Grundfos Pumps India Pvt. Ltd.                    

E-mail: mahathi@grundfos.com





    Facebook Twitter LinkedIn Technorati