PRESSURE BOOSTING MADE SIMPLE

17/08/2012

Hydro Multi B

Simplified Pressure boosting Pumps for Indian market

After successfully providing pump solution across different verticals in Indian markets, Grundfos pumps India Pvt Ltd introduces the complete range of Hydro Multi-B pressure boosting pumps. The Hydro Multi-B is a new Booster-set Product in line with “PRESSURE BOOSTING MADE SIMPLE” concept. The design for booster pumps is focused entirely on meeting the needs of ‘economy’ class market of India.

The brand new booster set product line - Hydro Multi-B is designed to simplify the Pressure boosting and best in class in terms of dedicated pump control. Hydro Multi –B is easy to operate as it is highly user friendly. They also meet the safety factor and it’s fast to install. Hydro Multi – B is easy for any installer as it is ready set pump with a remote start and stop. The booster pumps support 2 main applications firstly, keeping constant pressure in applications with varying flow needs such as commercial and domestic buildings. Secondly, there is a dedicated tank filling solution with special cascade ramp-up that protects the piping.

This new Hydro Multi-B which has been developed by conducting intensive discussions and survey with Building services market of India in the last 2 years. It was a main target for the Hydro Multi – B project to deliver a product- line that will be competitive, meeting the optimum demands of Indian customers.

The Hydro Multi-B line intends to lead a competitive range of Booster products, incorporating ‘high-efficient’ Horizontal stainless steel CM/CME range of pumps. The system has the discharge capacity, which is extended up to 40m3/hr and the head ranges up to 65 meter. In order to meet the needs of competitive market, different variants have been created such as All 306 stainless, galvanized steel, Multi-B/S version motors.






    Facebook Twitter LinkedIn Technorati