Convector

A convector is a heating surface that transfers heat mainly by convection. Convection is the process by which heat is transferred when cooler air flows over the warm surface of a solid material.

A convector is a heating surface that transfers heat mainly by convection. Convection is the process by which heat is transferred when cooler air flows over the warm surface of a solid material.

A convector consists of water-filled heating plates, fitted with corrugated fins, which create a very large overall surface area, thus increasing its ability to transfer heat to the air by convection. Over 90 % of a convector’s heat energy is transferred to the air by convection.

Convectors are often used in locations where there is not enough space for radiators. The amount of heat energy transferred by a convector will decrease if installed in locations where airflow is restricted. The heat transfer will decrease by approx. 20–25 % when installed in a recess, and by 15-20 % if located just below a ceiling. When a convector is fitted under a ceiling, there is also a risk of a large temperature gradient in the room, as a layer of warm static air forms under the ceiling. Lack of heat at floor level may be uncomfortable for the feet or increase the chance of floor draughts.


    Facebook Twitter LinkedIn